VED (Vertical Exhaust Duct)

The VED system transports warm airflows from the top of the (server) rack to a central cooling system using an air duct. The VED system is attached to the (server) rack with a specially designed roof plate. The upper part of the VED is telescopic and can easily be slid under the lowered ceiling. A packing seal at the top ensures a proper air seal, even if the lowered ceiling is not fully level!

Aisle Containment

Aisle containment is the solution to the challenges which data centers have been presented with since day one: the optimization of cooling and energy efficiency through the separation of hot and cold airflows. We divide two aisle containment solutions: Next Generation Corridor and Free Standing Corridor.

Aisle Containment

Aisle containment is the solution to the challenges which data centers have been presented with since day one: the optimization of cooling and energy efficiency through the separation of hot and cold airflows. We divide two aisle containment solutions: Next Generation Corridor and Free Standing Corridor.

Next Generation Corridor

The Next Generation Corridor is the ultimate answer to the ever increasing demand for flexible and modular solutions. In the form of the Next Generation Corridor, we lift modular thinking and energy-efficient data centre design to a higher level.

next-generation-corridor

Free Standing Corridor

When the highest amount of flexibility is required, the Free Standing Corridor is the most optimal solution. The Free Standing Corridor is a fully self-supporting aisle containment system, with which closed off aisles can be created independent from the IT-racks – which is not usual in the data centre market.

refroidissement passif

Discover more about the range